800xa 6.0 unable to add client
we are having only one server and client. system is in workgroup connected through unmanaged switch. when we are adding client in system config console it is showing disconnected. server is pinging from client. but when we are pinging client with ip address from server it is pinging but it is not pinging wheh I am pinging with client name.
suggest me what to do?
Answers
Check that Rnrp Works and Shows the Client on the Server (Click that "R" Icon in Taskbar). If not it could be your ip configuration doesn't follow the Rnrp Rules...?
>"but it is not pinging wheh I am pinging with client name."
So either DNS ( in a domain ) or hosts file ( in a workgroup ) is not setup to resolve the names properly. Fix this.
Add new comment