Server2012R2 Installation Strange Error
I prepare a package with using system planner and then I choose manuelly package installation..etc Now I had a strange error and installation was broken during 3rd party installation windows components and services. What can I do sometimes. I added SS.
PS. Installation 5.1 FP4 RevD
Voted best answer
Depending on from wich version you are comming you can restore your backup in version 6.0. Server 2012 is compatible with version 6.0. You should read the upgrade manual for version you are comming from to version 6.0. ABB released several upgrade manuals. E.g. 2PAA111694-600 System 800xA 5.1 to 6.0 Upgrade
Answers
Server 2012 is not supported for 5.1 FP4 RevD. Please start again using Windows Server 2008 R2
Can I set up rev6 full backup conversion possible?
Hi
Are you sure you can install 5.1 on server 2012?? coz v6 requires 2012 server and i have not seen 5.1 installed in 2012 server
Add new comment