TP800
I'v got turbine protection module TP800 (TBU810, CPM810, TPM810) phisically connected via profibus to CI854 module. But I have no idea how to connect them in Control Builder. I guess there should be some special Hardware Library, but not shure.
Voted best answer
I'm not sure if there is a hardware library, the TP800 comes with a GSD file which you might have to load into hardware library yourself.
Answers
Thought I'll find .gsd on one of the System 800xA DVD (Device Library PROFIBUS), but no. Asked this question to official representative - they send me TP800 .gsd and .hwd files.
Add new comment