FFupload aspect not found, Cannot Find Upload Entity
Dear All,
After succesfull Full Maintenance restoring the backup, in The HSE Subnet and also in FF Library not showing FFupload Aspect.
When we select the FFManagement Aspect its popping up with Message "Cannot Find Upload Entity".
Extensions already loaded.
Tried with Uninstallaing and reinstalling ABB Device Management for FF, but still the issue not solved.
checked the Log in the Configuration wizard and found message: Aspect 'FFUpload' on object XXXXXX Failed to unserialize itself. 80004005-Unspecified Error.
System : 5.1 FP4
Could anyone help to resolve this issue.
Thanks & Regards-
Answers
this can be resolved by performing the following steps.
1. Remove the Foundation Fieldbus system extension from Admin structure->Administrative Objects->Domains-><SystemName> Domain->System Extensions Aspect.
2. Delete ABB Device Management Foundation Fieldbus object, System Extension from Admin structure->Administrative Objects->Inventory Object->System extensions Aspect type->ABB Device Management Foundation Fieldbus object, System Extension
3. Uninstall the ABB Device Management Foundation Fieldbus software in Aspect server.
4. Install ABB Device Management Foundation Fieldbus software in Aspect server and load the system extension.
Add new comment