Device Integration Library for Compact Control Builder
Hi!
Is there a special Device Integration Library for Compact Control Builder or is it possible to use the same as for 800xA?
Or do you have to import for example the GSD-files your self?
Answers
Compact Control Builder has no support for a DTM architecture. meaning that the device object types of the device center which come with DTM frame (HART, Profibus) can not actually be used in CBM with that functionality, you can download eventhoughthe Device object type from DIC but you would only be able to use the .gsd part.
As you suggest only the .gsd can be imported into CCB. This means that for every Profibus device you want to use you would have to add in your Hardware Library in CCB a hardware object based on the .gsd you import.
Add new comment