Check 800xA V6 Compatible Hardware Modules without affecting production
Hi,
I would like to know if there is a way to check the hardware version of controllers, communication modules and IO Modules in an 800xA system without physically removing the cards and checking the sticker on them. There are known compatibility issues with certain versions of hardware when upgrading to version 6.0 that is listed in 2PAA111899-600* and since the system is in production, one cannot physically remove these units to check the PR:* versions.
The controller log only seems to show this info for certain CEX bus units and not even the version of the controller itself. The IO modules will also not be shown in the controller log.
How else can this be done?
Answers
Have you checked what CBM->Remote System->Controller Diagnosis->Get->IO module xxx can do for you?
FYI: this info among other is automatically extracted by the AC800MFingerPrint.exe tool
Add new comment