Faceplate Expression not working for Control Operation
Hi All,
This question is related to the previos ques which I asked a couple of days ago regarding the faceplate expressions for controlling the breaker, Isolator & Earth Swtich.
Issue is I am able to control the CB,ISO & ES using control selection & control operation from CET. Its working fine when I do the write command from the CET. however its not working in 800xA.
for simplicity I used the same expressions given in IEC61850 manual for CB, ISO & ES Control. but those expressions are also not able to provide the healthy status of buttons as shown in screenshot.
I see no other options other than asking the experts here. I can send the pcmi file via mail if required.
Please suggest something so that control operation is possible from faceplate.
Thanks & regards
Answers
This question has not yet been answered.
by lhmonaco Rank: 350 on 6/20/2016 4:17:10 AM | Like (0) | Report
Dear Yoginder,
Please add a screenshot of how the expressions are configured in your Faceplate buttons. Also, add screenshot of your configuration in the IED Signal Mapping aspect.
Add new comment