aSub-Tabs Disappering
Hi,
I have a problem with the sub-tabs which diseppears after going to another tab.
So (I will refer to attached pictures):
- if I open the Operator Workplace and go Aux tab then I can see all subtabs
- if I switch to another tab and then come back to Aux then all the subtabs under Aux are gone and I cannot get them until I restart the Operator Workplace.
- Is it happening just with Aux tab. If I switch in between the others tabs I get all the subtabs, and I dont have it all the time. For some days the subtabs diseppears and for some days I have them.
I cannot relate the problem with some display/grafical settings because nothing changes.
Dose anyone has any clue what can trigger the problem?
Thank you!
Answers
This question has not yet been answered.
Add new comment