Graphic Element shows missing in operator station of 800xA
we have upgraded a system from 5.1 to 6.0 . After upgrade one of the element goes shows missing in operator station .
Please see the screenshot.
we can see this element in plant explorer and it is working well. We can find this in graphic editor. This element is missing only in "operator Station " of 800xA 6.0 .This element is working well in 800xA 5.1 Fp4 RU2.
Any suggestion ?
Answers
Dissect the element; is it PG2, is it VB6?
Maybe this is a wrapped element requiring additional software to be able to presented on operator clients.
Hello,
we had this problem also, a working PG2 display in 5.1, upgraded to 6.0 did not work.
We found out that when Import the display to 6.0 then 6.0 can not handle "special characters" in the User Enumeration when importing. The solution we saw is to select the display element again in the Properties window.
/Ronny
Add new comment