more bdm templates in 800xa v5.1
how could I get more BDM templates for v 5.1 i know that some of them are obsolete
but it is written that I could update old templates to be compatible with v5.1
could some one please attach
- CBM_Applications.xls
- CBM_ControlModules.xls
- CBM_ControlModuleTypes.xls
- CBM_FunctionBlockDiagram.xls
- CBM_FunctionBlocks.xls
- CBM_FunctionBlockTypes.xls
- CBM_HWUnits.xls
- CBM_IO_Variables.xls
- CBM_Programs.xls
- CBM_SingleControlModule.xls
these excel workbooks ?
Voted best answer
NOTE: Though these work in 5.1 and later versions, ABB doesn't support these templates.
Answers
Hi
These templtes were removed in SV 5.1 onwards sighting the improper usage of the old templates.I would suggest you to raise this question to the R&D by contacting the local supportline.
Hello,
You can also make BDM as per your requirement as we are doing in our project.
We have made a set of templates and we are using them again and again.
We have made templates for Sil Access Control. IO Allocation, Parameterisation e.t.c
Basic Steps are as follow
Just right click on the project in which you want to run bdm.
Right Click-->Advanced -->Bulk data manager
An excel sheet will open now.Now Drag Drop the required data for which BDM is required.
For Example:-For Control Modules, Drag and Drop the control properties aspect.
This will open a pop-up of all the parameters.Select the required and then close the pop up.
After this Drag and Drop the project for which you want to run the BDM.Populate the sheet with required parameters.
To Upload:-
go to ADd-Ins on MS Excel and and click on Save all objects and then Uplaod all objects Icon.
This will run the BDM.Make sure controller is reserved by you while doing so.
If you need some specific information for BDM feel free to contact.
Best Regards
Add new comment