UPDATE FIRMWARE WITHOUT USING SD CARD(AC500)
Hello
I want update firmware for my cpu, but i dont have SD CARD.
can i do this without using SD CARD?? HOW?
Regards
Answers
Hi
IMHO the updating of FW is possible only with SD card and NOT without.
The cost of the adapter for SD card is very cheap.
The instruction are below
Hope this help you
Hi,
It is also possible to update CPU via FTP- for PLCs with on board Ethernet and FW2.1 upwards. (The SD card- as suggested earlier is easier!, but if you dont have access to one - follow the attached method)
Hi
If you have Automation Builder version higher than 1.2.0 you have direct option to download the firmware to PLC from Automation Builder with out using SD card.
Regards,
Denson
Add new comment