Installation path of Automation Builder 1.2.2.3375
Greetings!
I'm trying install newest Automation Builder version 1.2.2 Build 3375. Installer is not going after selecting of software packages to be installed on the Selection Page, because of low disk space of C: partition, but I have enough space on D: partition. Is it possible to change installation path of Automation Builder so that installer is looking for other partition, not C: ?
Thanks.
Voted best answer
In Automation Builder 1.0, each of the package are install individually which allow you to change the installation path.
For AB 1.1 onwards, all the package are group together during installation and the installation path are not allow to change.
Answers
The Automation Builder installation is only available on C: partition which is your OS partition.
Chooi,
Thanks. Does it mean that AB can be installed only on C: ?
Is this valid for previous versions of AB? V1.0 I've installed on E: partition.
Chooi,
Thanks.
hi,
Use AOMEI Partition manager to increase the space of local disk C.
Source: http://www.disk-partition.com/
Add new comment