Modbus Signals count as Controller IO license signals
In version 9.2 , modbus signals are counted like IO, and affect licese?
Voted best answer
Yes it does. This behaviour is not version dependend. It should do so in all previous versions. It was specified like this from the beginning of I/O count licensing.
Answers
Hello,
Yes it is, same you can test or cross verify by adding few modbus reg/coil to process station, clear pausibility check and hover over pointer on status line(check image below it can be found at lower right hand corner or cbf frame) you can find i/o count increased.
check more details @ http://www402.abbext.com/Freelance-License-q1277.aspx
by csanchez411
Freelance 9.2
Add new comment