SoftController Error
Hi,
When I download the Application to the softcontroller, the download dialog box appears with No error,
But after confirming download Notifications and when downloading, an Error appears (Picture NO 1),
When I click the "OK" button of this error then the softcontroller Stops and an other error appears (Picture NO 2),
what is the solution?
Thanks.
Voted best answer
Hello,
You may get abart whenever your machine is not connected to any switch/cross cable to any PC you can connect your standalone PC network to any temporary sw/any laptop then start softcontroller and download.
Answers
Hi,
If you are running only one SoftController in a machine, then pls put the IP as "172.16.1.1:2".
But in your screenshot it is mentioned as "172.16.1.1:4". This will aslo works but it required additonal settings as below
1.Launch Softcontroller; Goto Setup - System Variables, it will open the Popup called "Setup System Variables"
2.Type "mmsprocessnumber" in the "Variable" Input Field
3.Type "3" in the "Value" Input Field and then Press "Set"
4.Then Goto C/Program Files(86)/ABB Industrial IT/Control IT/SoftController 5.1
5.Run "slcmain.exe" application
Have you looked at the log file ?
What does it say ?
Hi, The Log file says:
Operating System Information
============================
Caption: Microsoft Windows 7 Ultimate
CSDVersion: Service Pack 1
Version: 6.1.7601
OSLanguage: 1033
ForegroundApplicationBoost: 2
LastBootUpTime: 20160510153237.091970+270
Computer System Information
===========================
Caption: SINGLEENGNODE1
Domain: WORKGROUP
Manufacturer: FUJITSU
Model: LIFEBOOK AH532/G21
Name: SINGLEENGNODE1
NumberOfProcessors: 1
SystemType: X86-based PC
Processor Information
=====================
DeviceID: CPU0
Caption: x64 Family 6 Model 58 Stepping 9
Manufacturer: GenuineIntel
Name: Intel(R) Core(TM) i5-3210M CPU @ 2.50GHz
CurrentClockSpeed: 2501
NumberOfCores: 2
NumberOfLogicalProcessors: 4
I 0000-00-00 00:00:00.000: Starting MMS Server
I 0000-00-00 00:00:00.000: MMS Server running
I 0000-00-00 00:00:00.000: MMS Server connected
I 0000-00-00 00:00:00.000:
I 0000-00-00 00:00:00.000:
I 0000-00-00 00:00:00.000: -----------------------------------------------------------------------------
I 0000-00-00 00:00:00.000: Product : Soft Controller
I 0000-00-00 00:00:00.000: Version : 5.1.0/0 (Build 5.1.48.40)
I 0000-00-00 00:00:00.000:
I 0000-00-00 00:00:00.000: Created : 2010-07-02
I 0000-00-00 00:00:00.000: ABB AB
I 0000-00-00 00:00:00.000:
I 0000-00-00 00:00:00.000: Working folder is: c:\softcontrollers\SoftController-4\Data
I 0000-00-00 00:00:00.000: Memory information
I 0000-00-00 00:00:00.000: TotalPhys = 2942 MB, AvailPhys = 1641 MB
I 0000-00-00 00:00:00.000: TotalPageFile = 5882 MB, AvailPageFile = 4074 MB
I 0000-00-00 00:00:00.000: TotalVirtual = 2047 MB, AvailVirtual = 2004 MB
I 0000-00-00 00:00:00.000: Heap size = 25 MB
I 2016-05-10 16:07:45.734: CodePage: 1252, Character set: ANSI - Western/Latin I
I 2016-05-10 16:07:45.734: Timer resolution 1 millisecond
I 2016-05-10 16:07:45.735: Reading systemsetup.sys.
I 2016-05-10 16:07:45.743: License Manager: Feature Name Control_Software
I 2016-05-10 16:07:45.744: License Manager: Version 5.1.0
I 2016-05-10 16:07:45.744: License Manager: Hardware ID 84-A6-C8-01-1F-DE
I 2016-05-10 16:07:45.748: Priority raised to high for Schedule.
I 2016-05-10 16:07:45.769: MMS Server is running
I 2016-05-10 16:07:45.797: Network address is 127.0.0.1:4.
I 2016-05-10 16:07:45.803: Current time zone: Iran Daylight Time
I 2016-05-10 16:07:45.803: Position Module Firmware Name Date Version
I 2016-05-10 16:07:45.803: 0 CONTROLLER OMEGA 2010-07-01 5.1.48.40
I 2016-05-10 16:07:45.804:
I 2016-05-10 16:07:45.832: Ready
I 2016-05-10 16:07:45.833: Priority raised to high.
I 2016-05-10 16:07:55.835: Session.Log read by other system. Size = 3063
I 2016-05-10 16:07:55.836: Init Log Saved
I 2016-05-10 16:08:01.730: Create applications definition domain
I 2016-05-10 16:08:01.817: Create controller configuration domain
I 2016-05-10 16:08:01.852: Protocol Handler Name = PhSimulation
I 2016-05-10 16:08:01.852: Version = 5.1.48.19 ; 2010-05-12
I 2016-05-10 16:08:01.852: Ph binary version = : 0x00000000
I 2016-05-10 16:08:01.853: AE System events to controller log: Medium Severity
I 2016-05-10 16:08:01.893: New I/O-connections configuration.
I 2016-05-10 16:08:01.893: I/O-connections configuration waiting for application/s.
I 2016-05-10 16:08:03.001: Create application instance domain: R615984491Application_1
I 2016-05-10 16:08:03.051: Create application R615984491Application_1
E 2016-05-10 16:08:03.094: ErrorHandler PM: Assertion:StrOwner (2,5,ER)
************************************************************
E 2016-05-10 16:08:03.094 EXCEPTION_ACCESS_VIOLATION at 0x00446fed
CREATING A MINI DUMP FILE:
Saved dump file to 'c:\softcontrollers\SoftController-4\Data\SoftController 2016-05-10 16.08.03.094.dmp'
DUMPING REGISTERS:
EBP : 0x0012fbc0 : fc64 0012 9d46 0044 cddc 0227 fd48 0012 : d···F·D···'·H·&m
iddot;·
EIP : 0x00446fed : b60f 5c51 d285 0575 26e8 189e 8b00 fc45 : ··Q\··u··&···
;·E·
CS : 0x0000001b
FLAGS: 0x00010202
ESP : 0x0012fbbc : 0000 0000 fc64 0012 9d46 0044 cddc 0227 : ····d···F·D·&mid
dot;·'·
SS : 0x00000023
EDI : 0x0012fc64 : fc80 0012 9bd2 0044 cddc 0227 fc78 0012 : ······D···'&midd
ot;x···
ESI : 0x0012fd50 : fd60 0012 0003 0000 fec0 0012 5175 0053 : `·········&middo
t;·uQS·
EBX : 0x7ffd5000 : 0000 0000 ffff ffff 0000 0040 7880 7721 : ··········
;@··x!w
EDX : 0x0227acac : 6f69 3a6e 7453 4f72 6e77 7265 2020 0000 : ion:StrOwner ··
ECX : 0x00000000 : **** **** **** **** **** **** **** **** : ****************
EAX : 0x00000000 : **** **** **** **** **** **** **** **** : ****************
GS : 0x00000000
FS : 0x0000003b
ES : 0x00000023
DS : 0x00000023
DR0 : 0x00000000
DR1 : 0x00000000
DR2 : 0x00000000
DR3 : 0x00000000
DR6 : 0x00000000
DR7 : 0x00000000
ControlWord : 0x0000027f
StatusWord : 0x00000120
TagWord : 0x0000ffff
ErrorOffset : 0x0065c292
ErrorSelector: 0x0000001b
DataOffset : 0x0012fcf8
DataSelector : 0x00000023
Cr0NpxState : 0x00000000
DUMPING THE STACK:
0x0012fbbc : 0000 0000 **** **** **** **** **** **** : ····************
DUMPING THE CALL STACK:
Note: This call stack contains no static routines
The symbols shown are the closest match of global routines in the map file
For a more accurate result, use the dump file
Address Symbol
Call at 0x00446fed GetNrOfAlarms in PROGCONTROL
Call at 0x00449d46 CreateProgramHeavyPart in PROGCONTROL
Call at 0x00449bd2 CreateProgramLongJob in PROGCONTROL
Call at 0x005c69cc PollLongJobs in CONEVENT
Call at 0x005c6eb0 UpdateSubSystems in CONEVENT
Call at 0x00535175 sgMain in MAIN_SLCNT
Call at 0x00531c8d ? in
Call at 0x00663f8a ? in
Call at 0x76d13c45 ? in (C:\Windows\system32\kernel32.dll)
Call at 0x771a37f5 ? in (C:\Windows\SYSTEM32\ntdll.dll)
Call at 0x771a37c8 ? in (C:\Windows\SYSTEM32\ntdll.dll)
I 2016-05-10 16:08:03.366: Open handles: 186, GDI objects: 9, User objects: 2
Add new comment