800xA ver 6 - Installing .NET Hotfix
Hi,
Section 2 in the Installation manual for version 6, mentions installing of the .NET 4.5.2 hotfix. This was unsuccessful, rendering in error: HRESULT 0x80240017 (see appendix).
Remedy?
BR
Answers
Are you installing this hotfix after updating to 6.0.1? If so, then it should work. The error points that this hotfix is not applicable for you, possible reason could be that dot net 4.5.2 is not installed, which was available as an update in 6.0.1
Add new comment