Digivis500 AC500 library available for Freelance Operations
It has been brought to my attention by members of the ABB PACT division, that the AC500 library previously exclusive to Digivis500 is now also available in Freelance Operations.
However, I am unable to find anything. Could someone be able to point me in the right direction?
I am using the 2016 version of Freelance.
Answers
Have a look in your Export directory under the Freelancre installation directory. Look for a file called "AC500 Standard TagTypeLibrary V1.0.prt". Import this file with block import into the Freelance engineering tool.
The current file might not be the latest one. Freelance 2016 SP1 should contain an updated version of that file. You can also try to import the file delivered with DigiVis 500 if you have access to such an installation. Previous Freelance versions could not import this one, but the Freelance 2016 import has been enhanced to allow importing of DigiVis 500 project files.
I found that the AC 500 Tag Type library delivered with Freelance is different (only small changes) from the one delivered with DigiVis 500 (though both have the version 1.0). I attach the one with the most recent date stamp, which is the one delivered with DigiVis 500.
Add new comment