HART DTM File.
What is the solution if i dont get a dtm file from ABB solutions bank.
I need a HART DTM file for foxboro IADP10 pressure transmitter.
Voted best answer
Hello,
You can get required DTM file from vendor or google it. Only difference if dtm is available in solution bank it is tested with ABB control systems at device integration center and you have smooth device integration. as answered above you can check with DIC team.
One more possibility if you are not able to get device specific dtm file you can use generic hart dtm available at solution bank.
Answers
HART DTM should come along with the Device if you have procured it. If you can you can ask vendor(Foxboro) to supply the DTM file.
Check the below link. You can download it.
http://iom.invensys.com/EN/Pages/Foxboro_MandI_DocTools_DeviceManagers.aspx
Regards
Bharat Kahate
Add new comment