i do have an error when down load the application program
Greetings
I think I do have problem in the AC500 PLC
the CPU I do used is the PM564 -ETH
i do mange to connect t0 the CPU
but just i download the application i d do have an error (red LED light constantly )
the error code is (15656474)
notes that
I do rebuild the application both in the Codesys and the Control builder Plus
the station I do use is PM564 CPU and DX561
Voted best answer
Hi..
With reference to your errror no. It is indicating the created PLC configuration not matching with the actual configuration.
Please check.... and also acknowledge & clear the error in online.
Answers
Hello Sir,
I could not find the above mentioned error number in codesys. Please send the screen shot.
Greetings
sorry for inconvenient
the correct number shall be (151656474)
Regards

Sir,
Please help me to solve this error
how can I generate database of runtime error listing.?
AC-500 Serise PLC PM 591 for implemntaion
Add new comment