How make redundancy in scada using digivis?
Dear All
i would like to make redunancy in scada (using dgivis). i have two plc(AC500) , in plc part redunancy over.but now i need to scada redunancy .if anybody know that procedure please share your idea's
Thanks in advance
Voted best answer
Digivis 500 Operator stations will work in parallel and will fetch the real-time values from Codesys OPC server. Configure Codesys OPC server in a separete system, so that even if one Operator station is down the other OS will function with full functionality.
Answers
Two Digivis500 Operator Stations can work independently taking data from PLC through same OPC Server. Full redundancy for CodeSys OPC Server is not supported.
Add new comment