IEC61850 OPC Server Configuration
Hi Everyone,
I connect to 800xA System via IEC61850 OPC Server with REF615 relay,and I add new REF615 relay,I want to comunicate them but there is an uploader error which is attached file.I upload all device parameter by PCM600 tool,but I didn't comunicate between new devices to OPC Server like before.How can fix the problem?
Voted best answer
Hi,
it seems like you are directly trying to upload the scd file in IECUploader. it will not work. if you want to add a new relay to already existing project, then you have to do a little work in CET. open your previos project in CET then create a New OPC server (see pic 1)& import your new scd file here (remember the IEC61850 DA Server Instant) then you have to create a new opc server in control strucuture (pic 2). there you try to import your scd file for new relay. it should work.
Add new comment