Do anyone know what error code 30000F02 means?
We have an 902F CPU running in a plant. Two different times have the CPU make an unexpected restart. No programming activity or downloading have taken place with these two occations.
There are errors from 16.03.2016 and 18.12.2015 at issue.
Defect History
*****************************
Fatal Error Buffer:
01.01.13 00:00:07 Error 30000F89 in <_stb> at 00031E5C
18.12.15 07:39:19 Error 30000F02 in <_phy> at 0000D0DC
04.03.16 09:54:52 Error 30000F02 in <ROOT> at 00000500
Håkan Abrahamsson
Voted best answer
Hello Hakan,
in order to explain this issue we do need more indications :
# the whole controller logs (txt-file)of all the affected controller(s)
# the system error log from the use HMI (VIS?)at the time when these 2 errors occured.
# please send your answer to the Freelance Supportline in DE :
de.automation.supportline@de.abb.com and cc to me : dominique.deschamps@de.abb.com
best regards
Dominique
Add new comment