800xA workplace startscreen
during the workplaces start on the upper left side of the start screen the customer name will be displayed twice.
Who can provide the reference to the two strings?
The upper string corresponds to the parameter CUSTOMER_NAME from the license .sla file, but where can I find the reference of the second string?
regards, nola2k
Voted best answer
Hello nola2k,
Those strings that you mention are not something that you can "edit by hand", this information are read from the license file (.sla).
It is possible to change it but then you have to do it in SOFA and change the CUSTOMER_NAME and generate a new licensefile and load it to the system.
However there will always be two identical rows due to a bug in the system so "position1" and "position2" as you mention them will always populate the same information, which should be fixed in a future version.
Incase of those fields beeing empty that could mean that you don't have an licensefile, unable to read the license file, not able to contact the CLS server.
Answers
Thanks for your helpful answers,
but i mean the splash screen during loading the workplace.
Please see the attached picture.
When i start a workplace on a workstation (on aspect server both positions are free)
in both positions strings are displayed.
I need the source references for these strings.
Can you help?
regards, nola2k
Add new comment