VB6 vs PG2 graphic difference report
A life science customer wants to upgrade a 5.0 800xA system to 6.0.1 but will have to convert their current VB6 graphics to PG2, which will cause them to have to re-validate all of their graphics. Is there a way to get a difference report of the 2 graphics (original VB6 vs converetd PG2) to help lower the amount of retesting needed to revalidate a converted graphic?
Answers
Hello,
when using VB Migration tool, you get a difference report, and everything mentioned there has to be fixed/verified by you.
If you are sure that the VB displays are OK, ie running Consistency Checker without problems, then there are less problems after conversion....
/Ronny
Add new comment