Getting SIGMA Warning in back up :- xA5.0 Sp2 to 5.1 FP4 upgarde MOD 300
Hi,
After upgrading the system from 5.0 Sp2 to 5.1 FP4 with mod connect i have tried to take a maintenance back up. Back is completed with the below 4 warnings.
[Warning] Failed to get context property: "SIGMA_PROJECT_DIR"
[Warning] Failed to get context property: "SIGMA_DATA_DIR"
[Warning] Failed to get context property: "SIGMA_DATA2_DIR"
[Warning] Failed to get context property: "SIGMA_TEMP_DIR"
Kindly suggest me to remove the same.
Thanks and regards
Prashanth BS
Answers
Hello,
Many threads are there in AKS related to this, search for this.
Generally you will get this warnings when your redundant aspect partner is down.
Ensure your redundant aspect server is up and healthy,you can check this via system viewer or service status viewer in service str, and try taking the back up again.
If you have performed this upgrade activity in single node machine and trying to restore to the actual machines then no harm in restoring backup with these warnings once your all aspect servers becomes up and running these warnings will clear out from backup log.
Dear harsha,
I tried with the redundent Aspect server is on line but still i am getting the same error.
Kindly suggest me is there any other cause.
Thanks and Regards
Prashanth BS
When having a redunant server system, make sure that the service called:
Remote Registry
is started and is in Automatic in both PCs.
When making the backup, the server is trying to read entries inside the Registy of the other PC.
Add new comment