Bulk Configuration Manager - Microsoft Visual Basic - Automation Error / Unspecified Error
Hello,
I've recently loaded last ABB Qualified Windows Updates in a 800xA System SV5.0 SP2 RevD with Microsoft Office 2003 and after that, in an specific node (Harmony Connect & Config Server) the Bulk Manager Configuration is not properly working anymore. Excel crashes with error pop-up: Microsoft Visual Basic - Automation Error / Unspecified Error (check attached image).
I've saw Microsoft KB2687441 that matches pretty much with the historic and symptoms but it's applied for Office 2007.
http://support.microsoft.com/kb/2687441
Have you experienced errors like this?
Best regards,
Marco Camargo
Answers
Just an update if somebody else experience this situation in the future, it was fixed by unistalling “ABB Inform IT – Data Direct”, installing it again from the original system DVD and loading DataDirect Add-In back into Excel.
Add new comment