800xA v6.0.1 RNRP setup on Domain Controllers
Hi I'm following the manual (2PAA111708-600_E) page 49 and manually installs the
1.: ABB 800xA Common 3rd Party
2.: RNRP
But RNRP on the Domain controller do not see all the 800xA nodes. It's like some setup is missing.
Using the RNRT utility option 6 (find nodes with rnrp on one network shows all the other 800xA nodes - but the RNRP Event monitor do not show anything on the DC or on the other 800xA nodes.
All node has only been prepared with the NPT - no system has yet been configured.
Voted best answer
Ensure that following rules are configured on Domain controller after installing the RNRP.
Answers
Firewall exclusion is probably missing.
Check how RNRP (rnrpsvc.exe, rnrpmonitor.exe, etc) is exempted from Windows Firewall in some of the other aspect or connectivity servers. You probably need to add this exception manually in the domain controller.
Add new comment