Working with a HOPF GPS 6841 with RS-232, how do I time Sync a controller on the COM 3?
I am working with an installed system where I have a HOPF GPS 6841 which supports RS-232. It does not have an Etnernet Port. I want to sync a controller PM 8XX connected to the 800xA system. I cannot as of yet find any documentation that would help me configure the controller to be a SNTP slave of the GPS over the RS-232 port? I have a detailed understanding of the ABB 800xA Time Sync procedure with CNCP. Any help or documentaiton reference would be highly appreciated.
Answers
You will have to develop by yourself the protocol for receiving the time from the HOPF GPS using the serial port of AC800M and the control builder serial lib.
Using this method the precission you will get is not very good.
Add new comment