Advant Online Builder start fail after password change
The system is 800xA 5.1 Rev.E with advant connectivity. The engineering client use the PU410 of one connectivity server. The user is "800xAInstaller". All works fine. After a password change I get the error "The server process could not be started because the configured identity is incorrect. Check the username and password. " if I try to start the online builder. Start the online builder at the connectivity server is still possible. This error is not mentioned in the installation manual. I get the same error if I use "Test Server" from the Enineering Board Setup in the client.
Is the password stored? I have searched the registry without success.
Has anyone a suggestion?
/Erik
Answers
Hi
Plz tell which user password you have changed ?
Did you change the Service account password or Installer account password ?
Where did you change?
I could post pictures not in a comment:
But the Identity Tab use a different user, a local user which seems to be generated by the installation.
Add new comment