AdvaSoft Start up error
Problem:Solution
A description of this resolution:
"AdvaSoft Start up error" resolves the following:
A description of this resolution:
- AdvaSoft Start up error
"AdvaSoft Start up error" resolves the following:
- AdvaSoft Start up error
Application area: Water Treatment
Everytime I start up FIX , there is always an error dialog " TEXT ERROR (C:\WDMACS\NLS\flsglob.DOV) :Unable to open file " . So I click OK botton, it keeps continue start up until completely start . It is working well , but I just wonder why an error dialog appear in the begining and how to solve it . Every comments are welcome. I'm using AdvaSoft 1.3/3 .
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment