Using TEXTCOMB = 17 in EVENT DB element .
Problem:Solution
A description of this resolution:
A description of this resolution:
- Using TEXTCOMB = 17 in EVENT DB element .
"Using TEXTCOMB = 17 in EVENT DB element . " resolves the following:
- Using TEXTCOMB = 17 in EVENT DB element .
Engineering Platform : AS 500ES
Application area: Oil & Gas
I' m using Genusd (GU2,GU3,GU4,GU5) in AC450 and EVENT DB elements in the OS 1.8/2 with the textcomb=17 .
Should work in the following way in the alarm list: NAME
20chDescription
20chProperty Text
20chEvent Text
20chDate/Time
20chNAMEUser defined property textUser defined event textDate/TimeTextcomb=17
BUT it works in the following way :
NAME
20chDescription
20chProperty Text
20chEvent Text
20chDate/Time
20chNAMEUser defined property textUser defined event textDate/TimeTextcomb=17
So I don't have 28ch but only 8ch for the user defined property text in the alarm list.
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment