Compaq and AdvaBuild Eng Board Set-up
Problem:Solution
A description of this resolution:
"Compaq and AdvaBuild Eng Board Set-up" resolves the following:
A description of this resolution:
- Compaq and AdvaBuild Eng Board Set-up
Please refer to Status Report: SR-8071 AS 100 ES hardware part.
"Compaq and AdvaBuild Eng Board Set-up" resolves the following:
- Compaq and AdvaBuild Eng Board Set-up
Engineering Platform : AS 100ES
Application area: Oil & Gas
We've put an AdvaBuild Engineering Board in to a Compaq Deskpro EN Series 6400 and loaded AdvaBuild s/w. We have the old chestnut that the application can not see the co-processor. We have tried the obvious by disabling the sound - does anyone else have any ideas about other set-up parameters that may have to be changed for these Compaqs ?
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment