Use of the ONB Command DDB (Delete DataBase)
A description of this resolution:
- Use of the ONB Command DDB (Delete DataBase)
"Use of the ONB Command DDB (Delete DataBase) " resolves the following:
- Use of the ONB Command DDB (Delete DataBase)
Does anybody, out there, have any experience with problems that may be associated to the ONB DDB command.
We have recently experienced a problem whereby 10 DICs have been deleted and left a gap in the LF8 Concepts. Subsequently (possibly several days later and after more database - of different concept types - as been created) we have tried to load some more DICs. The TRBDS command has tried to load the new DICs into the locations where the concepts had been deleted - it managed to put the first one in.
However, the load failed with the error message: "Illegal Physical File - File not Defined" and "D/B Population - Database in disorder". TRDBS and CRDB for DICs now result in the same error messages.
To recover we are having to reload the entire node from Source Code, which, will take is most of the weekend because it is big.
I have suspicions that somehow DDB is to blame.
- Article imported from the previous version of KnowledgeBank
Add new comment