Master Gate 230
Problem:Solution
A description of this resolution:
"Master Gate 230" resolves the following:
A description of this resolution:
- DSCS 140 Setup
The (4) DSCS 140 cards must be configured for network and node. MasterBus 300 cards one and two should be configured for network of the first MP200/1controller and node number 127. MasterBus 300 cards three and four should be configured for network of the second MP200/1 controller and node number 127. Strapping groups are as follows: S5 defines bit 0-3 of the node number. S6 defines bit 4-7 of the node number. S9 defines bit 0-3 of the network number. S8 defines bit 4-7 of the network number.
"Master Gate 230" resolves the following:
- Master Gate 230
We have implemented a master gate 230 based on two controller DSPC 172-H and 4 modules DSCS 140. The switches of the DSCS140 are all set to 0 ( S5, S6, S8, S9 ). When starting the controller and getting it to position P1 and B1 I could not establish a connection of my network(controllers are in auto mode. There is no communication between the 2 connected nets.
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment