Advant Controller 410/450 and MasterPiece 200/1 - Handling of timers and delays in AMPL.
Problem:Solution
A description of this resolution:
"Advant Controller 410/450 and MasterPiece 200/1 - Handling of timers and delays in AMPL." resolves the following:
A description of this resolution:
- Let all PC elements, which have timers and/or delays, execute every cycle.
[ref SR2057 VASMASOITA0146 ]
"Advant Controller 410/450 and MasterPiece 200/1 - Handling of timers and delays in AMPL." resolves the following:
- A PC element with active timers and/or delays must execute every cycle to get a proper function
All PC elements which include timers and/or delays use the cyclic execution of the structure element (CONTRM, SEQ or MASTER). A PC element with active timers and/or delays must execute every cycle to get a proper function. If not the time will be erroneous; usually too long.
PRODUCTS CONCERNED
All releases/revisions of MasterPiece 200, MasterPiece 200/1 and Advant Controller 410/450.
SOFTWARE CONCERNED
All releases/revisions of basic system software:
MPxxx SW, XMPxxx SW, QMPxxx SW, QACxxx SW, QC01-BAS11 and QC02-BAS21
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment