Advant Controller 450 - Error in manual: User’s Guide, Advant Controller 450
Problem:Solution
A description of this resolution:
"Advant Controller 450 - Error in manual: User’s Guide, Advant Controller 450" resolves the following:
A description of this resolution:
- Which protocol to be used is not decided upon. Any communication facilities will be announced later in the Product Guide or the ordering documentation.
[ref SR5042 VASMASOITA0155 ]
"Advant Controller 450 - Error in manual: User’s Guide, Advant Controller 450" resolves the following:
- Documentation error
Today (1995-05-24) we do not provide any communication between Advant Controller 410/450 and the weighing system. (Otherwise it is not announced in the Product Guide).
Chapter 1.8.7.2 Applied Communication Table 1-21 indicates the use of RCOM for communication with weighing system MasterPiece 100W/100WM. This is wrong.
The same erroneous information is given in Chapter 3.1.6.2 Applied Communication Table 3-8.
Product concerned
Advant Controller 450*1.0
Manual concerned
User’s Guide Advant Controller 450, 3BSE002415R0001 Part 1 and 2
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment