On-line Builder*2.3 in AdvaCommand version 1.7, Only Postscript printers are supported
Problem:Solution
A description of this resolution:
"On-line Builder*2.3 in AdvaCommand version 1.7, Only Postscript printers are supported" resolves the following:
A description of this resolution:
- N/A
[ref SR7046 VASMASOITA0159 ]
"On-line Builder*2.3 in AdvaCommand version 1.7, Only Postscript printers are supported" resolves the following:
- INFORMATION ONLY
The On-line Builder*2.3 in AdvaCommand version 1.7 does not any longer support the line printers. It only supports Postscript printers. The line printers has no support in the MainWin libraries that are used to port the On-line Builder*2.3 from NT to UNIX.
PRODUCTS CONCERNED
AdvaCommand version 1.7.
SOFTWARE CONCERNED
AdvaCommand version 1.7 for ABB Master with the following description and designation:
AdvaCommand Software
Version: AS500OSBAS03*1.7
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment