AdvaCommand for Unix, Version 1.8 Revision 4. Errors corrected in Patch 02 (Service Pack 02)
Problem:Solution
A description of this resolution:
"AdvaCommand for Unix, Version 1.8 Revision 4. Errors corrected in Patch 02 (Service Pack 02)" resolves the following:
A description of this resolution:
- Corrected in Service Pack 2 (OS1.8-4-PATCH_02)
• The ‘patch’, or more correct ‘service pack’ since it is a collection of several patches, can only be installed in AdvaCommand 1.8 revision 4. If a customer has an error described below in AdvaCommand 1.8 revision 0, 1, 2 or 3, the customer first has to load 1.8 revision 4, before the service pack can be installed.
• Note! Once this patch/service pack has been installed it can’t be removed. If you, for some reason, want to remove the patch after it has been installed you have to install the AdvaCommand 1.8/4 from the beginning and then restore your station backup.
[ref SR1073 VASMASOITA0195 ]
"AdvaCommand for Unix, Version 1.8 Revision 4. Errors corrected in Patch 02 (Service Pack 02)" resolves the following:
- Alarm handling
Acknowledge of a process object fails when the Alarm list dialog is active.
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment