Advant Operator Workplace, AdvaCommand for UNIX - Version 1.8, Revision 4, Patch 1 (OS1.8-4-PATCH_01)
Problem:Solution
A description of this resolution:
"Advant Operator Workplace, AdvaCommand for UNIX - Version 1.8, Revision 4, Patch 1 (OS1.8-4-PATCH_01)" resolves the following:
A description of this resolution:
- Patch OS1.8-4-PATCH_01
• A patch to correct the errors described above is available for AdvaCommand for UNIX version 1.8 revision 4. The patch identity is OS1.8-4-PATCH_01
• The patch can only be installed in revision 4. If a customer has an error described below in AdvaCommand 1.8 revision 0, 1, 2 or 3, the customer first has to load 1.8 revision 4, before the patch can be installed.
[ref SR1025 VASMASOITA0215 ]
"Advant Operator Workplace, AdvaCommand for UNIX - Version 1.8, Revision 4, Patch 1 (OS1.8-4-PATCH_01)" resolves the following:
- Alarm and Event handling in AdvaCommand for Unix, Version 1.8
The milliseconds part in the time presentation was not correctly rounded when alarms were printed.
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment