MasterPiece 200/1 Error in PC element CONV-IA. Command DIBM or EBM
Problem:Solution
A description of this resolution:
"MasterPiece 200/1 Error in PC element CONV-IA. Command DIBM or EBM" resolves the following:
A description of this resolution:
- See WORKAROUND and REVISION
WORKAROUND
Don’t use this element in the Products and Software concerned.
REVISION
The software error will be corrected in the next revisions of MasterPiece 200/1*2.1 and MasterPiece 200/1*3.0.
[ref SR2004 VASMASOITA0274 ]
"MasterPiece 200/1 Error in PC element CONV-IA. Command DIBM or EBM" resolves the following:
- Error in PC element CONV-IA. Command DIBM or EBM
When the command DIBM or EBM is given to a PC program which contains an element CONV-IA, the element writes uncontrolled in the internal structures.
Result:
Strange functions in other PC element can occur.
PRODUCT CONCERNED
MasterPiece 200/1*2.1/x x = 0,1......11
MasterPiece 200/1*3.0/y y = 0,1......8
SOFTWARE CONCERNED
XMP200 SW*4.0/t t = 0,1......10
QMP220 SW*5.0/u u = 1,2......7
QMP240 SW*5.0/u
QMP260 SW*5.0/u
QMP280 SW*5.0/v v = 0,1......7
QAC280 SW*5.1/w w = 0,1
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment