AC 110: EVS(T) handling only works for one EVS(T)
Problem:Solution
A description of this resolution:
"AC 110: EVS(T) handling only works for one EVS(T)" resolves the following:
A description of this resolution:
- Information only, there is no solution to the problem
[ref SR1063 VASMASOITA0409 ]
"AC 110: EVS(T) handling only works for one EVS(T)" resolves the following:
- AC 110: EVS(T) handling only works for one EVS(T)
The first EVS(T) element receives events from all EVS(S) elements with corresponding Source-Bus and Source-Station, because no check is done whether Ident of received event is the same as the ident specified at receiving EVS(T) element.
Operator Station may receive unexpected events.
PRODUCT CONCERNED
Advant Controller 110*2.3/0
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment