MasterView 850/1*5.0 and Tesselator - DSIH 71B Track ball with 3 pushbuttons
Problem:Solution
A description of this resolution:
"MasterView 850/1*5.0 and Tesselator - DSIH 71B Track ball with 3 pushbuttons" resolves the following:
A description of this resolution:
- INFORMATION
A modified track ball unit, DSIH 71B, with three push buttons is now available. This track ball only goes together with the keyboards for MasterView 850/1 release 5.0 and Tesselator keyboard DSIH 70, which are scheduled for delivery as from 1/8 1990. The matching keyboards are marked on the bottom cover by a label with the text ’GV1’.
For use with separate Tesselator systems, the functions of the keys must be specified on the order.
For MasterView 850/1*5.0, the functions of the keys are: SELECT, ACKNOWLEDGE and FIND CURSOR. The trackball is available with either English or Swedish text.
Another new function is now available in MasterView 850/1*5.0: It is now possible to use the track ball for activation of dynamic function keys. Simply put the cursor on the dynamic key field and press SELECT.
[ref TMP0206 VASMASOITA0332 ]
"MasterView 850/1*5.0 and Tesselator - DSIH 71B Track ball with 3 pushbuttons" resolves the following:
- MasterView 850/1*5.0 and Tesselator - DSIH 71B Track ball with 3 pushbuttons
PRODUCTS CONCERNED
MasterView 850/1*5.0
Tesselator
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment