Advant Controller 110*2.1, The status bits for the second AF100 are not set correctly in the system status DSP
Problem:Solution
A description of this resolution:
"Advant Controller 110*2.1, The status bits for the second AF100 are not set correctly in the system status DSP" resolves the following:
A description of this resolution:
- The problem will be corrected with revision AC 110*2.1/2
There is no workaround to circumvent the problem.
[ref SR7076 VASMASOITA0358 ]
"Advant Controller 110*2.1, The status bits for the second AF100 are not set correctly in the system status DSP" resolves the following:
- Advant Controller 110*2.1, The status bits for the second AF100 are not set correctly in the system status DSP
PRODUCT CONCERNED
AC 110 2.1
SOFTWARE CONCERNED
AC 110 BASE SW*2.1/x
where x = 0, 1
The status bits for the second AF100 are not set correctly in the system status DSP.
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment