AdvaBuild for Windows*1.0, 1.1, 1.2 with Function Chart Builder*4.0, 4.1, 4.2 - 32 MB Limit in ODB:
Problem:Solution
A description of this resolution:
"AdvaBuild for Windows*1.0, 1.1, 1.2 with Function Chart Builder*4.0, 4.1, 4.2 - 32 MB Limit in ODB:" resolves the following:
A description of this resolution:
- Workaround:
Don’t hold all PC programs of a big target (AC 450) in the FCB;
generate source code of a specific PC program and delete it in FCB, before backtranslation of another one, if the size of the ODB file approaches this limit.
[ref SR6038 VASMASOITA0440 ]
"AdvaBuild for Windows*1.0, 1.1, 1.2 with Function Chart Builder*4.0, 4.1, 4.2 - 32 MB Limit in ODB:" resolves the following:
- AdvaBuild for Windows*1.0, 1.1, 1.2 with Function Chart Builder*4.0, 4.1, 4.2 - 32 MB Limit in ODB:
PRODUCTS CONCERNED
AdvaBuild for Windows 1.0/0, 1.1/0, 1.2/0
SOFTWARE CONCERNED
AdvaBuild Function Chart Builder version 4.0/0, 4.1/0, 4.2/0
FCB terminates with message "Data release y doesn't match code release 1.1", if the ODB becomes bigger than 32 Mbytes.
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment