Advant Controller 70 - FCB 4.6 does not support OPT: Extended PC of AC 70 1.2
Problem:Solution
A description of this resolution:
"Advant Controller 70 - FCB 4.6 does not support OPT: Extended PC of AC 70 1.2" resolves the following:
A description of this resolution:
- Use FCB 4.7 or later.
[ref SR0025 VASMASOITA0501 ]
"Advant Controller 70 - FCB 4.6 does not support OPT: Extended PC of AC 70 1.2" resolves the following:
- Advant Controller 70 - FCB 4.6 does not support OPT: Extended PC of AC 70 1.2
FCB 4.6 does not support AC 70 1.2/0
The option extended PC elements of AC 70 1.2/0 is not supported by FCB 4.6.
PRODUCTS CONCERNED
Advant Controller 70 1.2
SOFTWARE CONCERNED
Advant Controller 70 1.2/0
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment