Advant OPC Server for Advant Fieldbus 100 Version 2.0 - DAT names with 20 character long names
Problem:Solution
A description of this resolution:
"Advant OPC Server for Advant Fieldbus 100 Version 2.0 - DAT names with 20 character long names" resolves the following:
A description of this resolution:
- OPC 2.0 Patch04
The error described above is corrected in the OPC 2.0 Patch04, i.e. a new WiaConfigMgr.dll file.
After installing Patch04, the Advant OPC Server for AF100 has no problem to configure DAT names with 20 character long object names.
Installation instructions
1. Make sure that you have administrator privileges on the computer.
2. Stop the Advant OPC Server for AF100 2.0. (Open the Services Dialogue, located in Start\Settings\Control Panel, select the Advant OPC Server for AF100 item and click on the Stop button.)
3. Backup the WiaConfigMgr.dll, normally located in c:\Program Files\ABB\OPC\bin folder.
4. Replace the WiaConfigMgr.dll with the new one included in the Patch04.
5. Restart the Advant OPC Server for AF100. (Open the Services Dialogue, located in Start\Settings\Control Panel, select the Advant OPC Server for AF100 item and click on the Start button.
[ref SR1080 VASMASOITA0511 ]
"Advant OPC Server for Advant Fieldbus 100 Version 2.0 - DAT names with 20 character long names" resolves the following:
- Advant OPC Server for Advant Fieldbus 100 Version 2.0 - DAT names with 20 character long names
The Advant OPC Server for AF100 cannot handle (configure) DAT names with 20 character long names. The maximum number of character to use are 19.
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment