AMPL Control Configuration 1.7/0 Installation Problem. Error message " Ordinal not found in MFC42.DLL ..."
Problem:Solution
A description of this resolution:
"AMPL Control Configuration 1.7/0 Installation Problem. Error message " Ordinal not found in MFC42.DLL ..." " resolves the following:
A description of this resolution:
- The problem will be fixed in the next AMPL Control Configuration release 2.0/0. See also Workaround
Workaround
Reboot WINDOWS and run installation procedure once again.
[ref SR0071 VASMASOITA0579 ]
"AMPL Control Configuration 1.7/0 Installation Problem. Error message " Ordinal not found in MFC42.DLL ..." " resolves the following:
- AMPL Control Configuration 1.7/0 Installation Problem. Error message " Ordinal not found in MFC42.DLL ..."
Error message " Ordinal not found in MFC42.DLL ... " during installation of ACC 1.7/0. The problem occurs, if an older version of MFC42.DLL is currently in use on the PC during installation.
As the result of this problem, the ACC components are not registered in WINDOWS and therefore do not work properly.
Products Concerned
AMPL Control Configuration 1.7/0
Software Concerned
AMPL Control Configuration 1.7/0
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment