AMPL Control Configuration, Application Builder - APB Installation Problem
Problem:Solution
A description of this resolution:
"AMPL Control Configuration, Application Builder - APB Installation Problem" resolves the following:
A description of this resolution:
- The problem will be fixed in the next ACC release. See also Workaround.
Workaround
– Install APB afterwards as client using NetSetup.
Please note: Un-install of this APB will not remove everything, because both installations (server and client) use the same key in registry here.
[ref SR0048 VASMASOITA0587 ]
"AMPL Control Configuration, Application Builder - APB Installation Problem" resolves the following:
- AMPL Control Configuration, Application Builder - APB Installation Problem
APB installation problem :
• When you install APB with license key " ACC Select " , APB is installed as server instead of local installation.
• When you use AMPL Control Configuration 1.7/0 CD1 to install APB on Operator Station, APB is installed as server instead of local installation.
PRODUCTS CONCERNED
AMPL Control Configuration 1.7/0
SOFTWARE CONCERNED
Application Builder version 2.7/0
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment