Function Chart Editor-FP*3.0/1, 3.0/0, 2.3/0, 2.1/0 - Gaps in DAT() references of a DS
Problem:Solution
A description of this resolution:
"Function Chart Editor-FP*3.0/1, 3.0/0, 2.3/0, 2.1/0 - Gaps in DAT() references of a DS" resolves the following:
A description of this resolution:
- The problem is fixed in the next release of the FCE ( 3.1/0 ).
[ref SR4001 VASMASOITA0603 ]
"Function Chart Editor-FP*3.0/1, 3.0/0, 2.3/0, 2.1/0 - Gaps in DAT() references of a DS" resolves the following:
- Function Chart Editor-FP*3.0/1, 3.0/0, 2.3/0, 2.1/0 - Gaps in DAT() references of a DS
The Command Oriented Functions ( QMA221 ) together with MP200 always remove gaps in references at REFx terminals, i.e. independantly of SORT_REF = NO or YES, the signals are packed without empty places. This is done during interactive input and TRDBS.
The FCE does this only, if SORT_REF=YES.
So you have to pay attention to :
For MP200 :
- All gaps are removed on the MP200
- The dumped source code from a MP200 has different references, if the original source code from FCE had gaps in references.
For MP90 :
- All gaps are removed in target code, i.e. the representation in source code differs.
- See also problem description above.
The following versions of MasterAid 220 software components are concerned:
Function Chart Editor MP 200 (QMA222) version 3.0/1, ... 2.1/0
Function Chart Editor MP 90 (QMA223) version 3.0/1, ... 2.3/0
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment