Function Chart Editor-FP*3.0/1, 3.0/0, 2.3/0, 2.1/0 - MP90 online changes in big PC programs
Problem:Solution
A description of this resolution:
"Function Chart Editor-FP*3.0/1, 3.0/0, 2.3/0, 2.1/0 - MP90 online changes in big PC programs" resolves the following:
A description of this resolution:
- The problem is fixed in the next release of the FCE ( 3.1/0 ).
[ref SR4001 VASMASOITA0604 ]
"Function Chart Editor-FP*3.0/1, 3.0/0, 2.3/0, 2.1/0 - MP90 online changes in big PC programs" resolves the following:
- Function Chart Editor-FP*3.0/1, 3.0/0, 2.3/0, 2.1/0 - MP90 online changes in big PC programs
Fatal error in Module CVREDCIN Pos 26110, Err. -543, Add Info 511 during target code generation in online editing [ reason is overflow in an internal data structure ].
This happens only in some rare cases ( very big programs with many multiple connections between executable units ).
The following versions of MasterAid 220 software components are concerned:
Function Chart Editor MP 200 (QMA222) version 3.0/1, ... 2.1/0
Function Chart Editor MP 90 (QMA223) version 3.0/1, ... 2.3/0
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment