Function Chart Editor-FP*3.0/1, 3.0/0, 2.3/0, 2.1/0 - Backtranslation of NodeStructure source code
Problem:Solution
A description of this resolution:
"Function Chart Editor-FP*3.0/1, 3.0/0, 2.3/0, 2.1/0 - Backtranslation of NodeStructure source code" resolves the following:
A description of this resolution:
- The problem is fixed in the next release of the FCE ( 3.1/0 ).
[ref SR4001 VASMASOITA0605 ]
"Function Chart Editor-FP*3.0/1, 3.0/0, 2.3/0, 2.1/0 - Backtranslation of NodeStructure source code" resolves the following:
- Function Chart Editor-FP*3.0/1, 3.0/0, 2.3/0, 2.1/0 - Backtranslation of NodeStructure source code
After backtranslation of a nodestructure ( .NSS ) with more than 1 PC program, only the last one has correct PC terminal connections; in all previous programs they are virtual, i.e. there are 2 visual effects in the function chart :
- all PC elements are shown in 1 row, with no direct connections
- If a PC element is deleted, the connections at the connected other elements still exist.
The following versions of MasterAid 220 software components are concerned:
Function Chart Editor MP 200 (QMA222) version 3.0/1, ... 2.1/0
Function Chart Editor MP 90 (QMA223) version 3.0/1, ... 2.3/0
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment